Biogas and biomethane production from sludge and waste
How waste is converted into biogas and biomethane through anaerobic digestion to support circular resource use and reliable energy supply
Kısaca
- Biogas production converts organic waste streams such as food waste, agricultural residues and sewage sludge into renewable energy through anaerobic digestion, supporting waste valorization, energy recovery and the circular economy.
- Biomethane is produced by upgrading biogas to remove carbon dioxide, moisture and trace contaminants, creating a renewable gas that can be injected into natural gas networks or used in industrial and transport applications.
- Successful biogas and biomethane production depends on maintaining stable process conditions, consistent gas quality and high plant availability to maximize energy recovery and operational efficiency.
How to turn organic waste streams into renewable energy?
Organic waste streams such as agricultural raw materials, food waste and sewage sludge are converted into biogas and biomethane through anaerobic digestion. By recovering energy from waste, biogas and biomethane contribute to decarbonization, reduce waste volumes and emissions, and improve energy security through locally generated, renewable energy that can support electricity, heat and gas supply systems.
From a process and operational perspective, biogas and biomethane plants are designed to balance biological stability, gas and energy yield and overall availability under highly variable feedstock conditions. Operators aim to maintain a stable digestion process that delivers consistent gas quality and energy efficiency while coping with changing feedstock composition, loading rates and regulatory constraints. Unlike purely mechanical processes, anaerobic digestion is inherently sensitive to disturbances, making process stability a primary objective alongside energy recovery.
Önemli gerçekler
Less than 5%
of organic waste streams
are currently used to produce biogas and biomethane.
Source: World Biogas Association
Biogas versus biomethane – getting the basics right
- Biogas is the raw gas mixture produced during anaerobic digestion. It consists mainly of methane, carbon dioxide, as well as water vapor and trace impurities. It is typically used on-site for heat and power generation.
- Biomethane is processed biogas: carbon dioxide, water and impurities are removed so that the gas meets defined quality specifications. Through this processing step, biomethane can be used as a renewable gas that is interchangeable with natural gas and can be fed into the grid, used industrially or utilized in transportation.
Feedstocks and circular economy
Biogas production is built around the use of locally available feedstocks such as sewage sludge, agricultural raw materials, food and organic waste, and agro‑industrial by‑products. By converting these organic streams through anaerobic digestion, biogas plants connect waste treatment, energy recovery and nutrient recycling in a single process. Organic materials that would otherwise require disposal are stabilized; renewable energy is generated and digestate nutrients can be returned to agricultural use (in some countries). This integration makes biogas production a practical example of the circular economy, where material cycles are closed and both energy and resources are recovered within existing regional systems.
Anaerobic digestion – the core process
Anaerobic digestion is the key biological process in biogas production and takes place in oxygen-free digesters, where microorganisms convert organic material into biogas. The composition of the resulting gas, which consists mainly of methane and carbon dioxide, depends heavily on the properties of the feedstock and operating conditions such as organic loading, temperature range and overall process stability. As a biologically controlled and inherently sensitive process, anaerobic digestion reacts directly to changes in inputs and conditions: fluctuations in the feedstock or an unbalanced load can influence reaction pathways, reduce gas yield, cause variations in methane content, or lead to temporary process instability.
For this reason, digestion performance is not determined solely by design capacity, but by how consistently conditions are maintained within a biologically stable operating window - an essential prerequisite for reliable plant operation, particularly when treating mixed or seasonally fluctuating organic waste streams.
From biogas to biomethane
Upgrading biogas to biomethane involves removing impurities and non‑combustible components from raw biogas to raise its methane concentration to natural gas quality. After anaerobic digestion, the biogas is cleaned of hydrogen sulfide, moisture and trace contaminants. Carbon dioxide is separated using established processing technologies. This enables compatibility with existing gas infrastructure and broader end‑use applications, such as grid injection or use as a renewable fuel in transportation and industry.
Compared to direct biogas utilization, however, upgrading introduces additional process complexity and tighter operational requirements: gas quality specifications, energy consumption and process losses must be balanced against the benefits of grid compatibility and flexibility. As a result, upgrading represents a distinct operational step rather than a simple extension of digestion.
Gas quality, safety and process control
The gas quality in biogas and biomethane production must meet application-specific requirements, regardless of whether the gas is used for heat and power generation or processed for injection into the grid. Fluctuations in the composition of the feedstocks directly affect the gas composition and can lead to variations in methane content, moisture content, or pollutant concentrations.
Monitoring gas quality and process conditions is therefore not only a legal requirement but an essential component of safe and reliable operation: Early detection of deviations enables preventive measures and helps avoid abnormal operating conditions that could compromise plant integrity, plant availability or safety.
In practice, plant performance is evaluated based on the stability and consistency of key process outcomes rather than peak values alone, with consistent gas composition, stable fermentation behavior and reliable availability serving as key indicators of a well-managed biogas or biomethane plant.
Discuss your challenges with our expert
Our local Endress+Hauser industry experts are ready to support you.
Regulatory framework for the global use of biomethane
Biomethane deployment is governed by regulatory frameworks that define sustainability criteria, gas quality standards and market access. These frameworks establish rules for feedstock sustainability, lifecycle greenhouse gas emissions and certification, ensuring that biomethane qualifies as a renewable energy source. They also define requirements for grid injection, gas composition and quality to ensure compatibility with existing infrastructure and safe operation. In addition, regulatory systems include mechanisms for measurement, reporting and verification, as well as certification schemes that enable the tracking of renewable attributes and support market participation.
Biogas and biomethane production in practice
Get more insights to real projects demonstrating reliable production, process efficiency and regulatory compliance.