Title

Anahtar kelimelere, sipariş veya ürün koduna veya seri numarasına göre aramayı deneyin, örn. "CM442" veya "teknik bilgi"
Aramayı başlatmak için en az 2 karakter girin.

Raman upstream bioprocess control

Nicro delivers turnkey fermentation systems with real-time metabolite and biomass monitoring

Endüstri: İlaç
Rxn-45 probe, bioprocess manufacturing, real-time, cGMP, COP/SIP, large-scale bioprocesses

Özet

Nicro combined fermentation system engineering with Endress+Hauser Raman technology and analytical services from BICRO BIOCentre to create a complete solution for fermentation processes. Inline monitoring replaces time-consuming offline analysis with real-time measurements of metabolites and biomass. This gives scientists greater process insight, supports timely intervention, reduces contamination risk, and enables optimized production and increased yield.

The results: Faster, safer, and more productive fermentation

35

fermentation processes reached return on investment

33%

potential productivity increase over a 10-day period

The original cost analysis estimated a return on investment after 35 fermentation processes when inline Raman monitoring was compared with offline sample testing. The analysis also determined that the faster turnaround of Raman-monitored fermentation could increase plant productivity by 33% over a 10-day period.

Real-time insight improves fermentation control

Direct inline measurement of glycerol as an input metabolite, acetate as a byproduct, and OD600 for biomass growth provides deeper insight into fermentation performance. By monitoring multiple attributes through a single probe, the solution enables process decisions to be based on current conditions rather than delayed laboratory results. Results include:

  • Faster process cycle times through real-time metabolite monitoring
  • Improved process control supporting optimized production and increased yield
  • Reduced contamination risk by limiting offline sample handling
  • Simultaneous monitoring of multiple fermentation parameters
  • Reduced time between batches
  • A complete packaged technology solution for fermentation processes
Photo of Maja Marinović, PhD, Head of Microbiology Laboratory, BICRO BIOCentre Ltd

“Metabolic switch does not occur always at the same time, and online monitoring is the only way to know when exactly to intervene.”

Maja Marinović, PhD, Head of Microbiology Laboratory, BICRO BIOCentre Ltd

The challenge: Replace slow and risky offline analysis

Fermentation progress can be estimated by monitoring dissolved oxygen in the media. Optical density and metabolite concentrations provide additional insight, but these parameters have traditionally been measured offline using time-consuming chromatographic techniques.

Removing samples for analysis delays access to process information and introduces additional handling. It can also create a risk of contamination and the potential loss of a valuable batch. Nicro needed a solution that would provide timely information about metabolite concentration and biomass growth without relying on repeated offline sampling.

Our solution: Integrated Raman monitoring for fermentation

Nicro combined its fermentation engineering expertise with BICRO BIOCentre and Endress+Hauser technologies and services to provide a complete packaged solution for fermentation processes. The solution includes:

  • Engineering and design of a complete fermentation system from Nicro
  • An Endress+Hauser Raman Rxn analyzer
  • An Endress+Hauser Raman Rxn-45 probe
  • Analytical services from BICRO BIOCentre
  • S-PACT modeling services supporting analytical model development

The Raman probe is installed directly inline and monitors glycerol concentration, acetate concentration, and OD600 for biomass growth. Multiple attributes can be monitored simultaneously through one probe, providing a real-time view of fermentation conditions and eliminating the delay associated with offline sample analysis.

Inline information also helps scientists recognize process events that may not occur at exactly the same point in every batch. In the documented application, online monitoring allowed scientists to identify when bacteria switched from one carbon source to another, supporting intervention at the appropriate feed point.

Download the full case study

Want access to the full case study as a PDF?

Download a copy to read at your convenience, save for future reference, or share with colleagues.

Download the full case study

Bizimle irtibata geçin

Teklifimizle ilgileniyor musunuz? Uygulamanız hakkında görüşmek ister misiniz?

Lütfen size nasıl yardımcı olabileceğimizi mümkün olduğu kadar ayrıntılı biçimde bildirin. Bu şekilde size mümkün olan en iyi cevapla geri dönebiliriz.

Products and services used

/

Related solutions and technology

Optik analiz

Laboratuvardan proses uygulamalarına kadar gaz, sıvı ve katılardaki kimyasal bileşimi ve konsantrasyonu izlemek için optik analiz sistemleri.

Ayrıntılı bilgi

Atık su deşarjının izlenmesi 

Sürekli değerler sunan ve kirliliğe hızlı yanıt veren eksiksiz ve güvenilir izleme prosesi ile yasal sınırlar dahilinde atık su deşarjını gerçekleştirin.

Devamını okuyun

Doğal gaz boru hatlarında hidrojen ölçümü

Doğal gaz boru hatlarında Raman spektroskopisi kullanılarak yapılan hızlı ve sürekli hidrojen ölçümü, sarf malzemesi veya boru ağzının genişletilmesini gerektirmeden güvenli karıştırma, kalite uyumluluğu ve dinamik proses kontrolü sağlar

Devamını okuyun

Güvenilir ve yasalara uygun gaz enjeksiyonu için biyometan kalitesinin incelenmesi 

H₂S, suyun çiğlenme noktası ve güvenli şebeke enjeksiyonu sayesinde etkili çalışma için önemli olan parametrelerin hızlı ve doğru çevrimiçi ölçümünü gerçekleştirerek güvenilir biyometan kalitesini elde edin. 

Devamını okuyun

Tuz giderme işlemleri için çevrimiçi su kalitesi takibi sistemiyle ters ozmoz membranlarını koruyun 

Tuz giderme ve su tekrar kullanma uygulamalarında RO (Ters Ozmoz) membranlarını korumak, temizlik iş yükünü hafifletmek ve membran ömrünü uzatmak için güvenilir çevrimiçi su kalitesi takibi

Devamını okuyun

Kriyojenik Tanklarda (LNG, etilen, LPG ve amonyak) Sızıntı Tespiti

Kriyojenik tank sızıntılarını erken tespit edin ve durumu kontrol altında tutun. Endress+Hauser, insanları, varlıkları ve kritik altyapıyı korumak amacıyla sürekli ve son derece güvenilir sıcaklık izleme çözümleri sunar.

Devamını okuyun

Gerçek zamanlı CCUS ölçümü ve doğrulama

Karbon Yakalama Teknolojilerinin Geleceğini Keşfedin: Yoğun faz uygulamalarına özel, hassas ve güvenilir çözümler

Devamını okuyun

Uyumluluğu sağlamak için sürekli emisyon izleme çözümleri

Uyumluluğu sağlamak için sürekli emisyon izleme çözümleri

Ayrıntılı bilgi

FAQs

Company logo of: Nicro

Nicro is a Croatian company whose tailored bioreactors propelled the rise of pharma, biotech, food and chemical industries in the region.